Support-Portal » Conditionsfile (en)

General information

It is possible to also incorporate conditions and content for the existing catalogue via a separate CSV file. In this way, prices, bulk prices, delivery times, customer-specific labels, customs tariff numbers, etc. can be added to the catalogue and replaced there.

Important: A catalogue (BMEcat) must be provided at least once! The conditionsfile does not work without a basic catalogue.

Creation and structure of a conditionsfile

You can create the conditions file using Microsoft Office (Excel). The following column headers and thus information are possible:

Column name Description
SUPPLIER_AID Supplier item number (mandatory)
ARTICLE_REFERENCE1 Item number for the reference item
ARTICLE_REFERENCE1|type Type of reference item (similar, accessories, others)
BUYER_AID1 Customer specific label
BUYER_AID1|type Value of the customer specific label
CONTENT_UNIT Content unit
DELIVERY_TIME Delivery time
DESCRIPTION_LONG Long description
DESCRIPTION_SHORT Short description
EAN EAN
FEATURE_NAME Feature name
FEATURE_UNIT Feature unit
FEATURE_VALUE Feature value
KEYWORD Keyword
LOWER_BOUND Price scale boundaries in price scales
MANUFACTURER_AID Manufacturer number
MANUFACTURER_NAME Manufacturer name
MIME_SOURCE Image/pdf name
MIME_TYPE File type
NET_CUSTOMER Customer price
NET_LIST Mercateo purchase price
NO_CU_PER_OU Packaging quantity (number of content units per order unit)
ORDER_UNIT Order unit
PRICE_QUANTITY Price quantity
QUANTITY_INTERVAL Quantity scale
QUANTITY_MIN Minimum order quantity
REFERENCE_FEATURE_SYSTEM_NAME1 Classification system name
e.g. ECLASS-5.1.4, ETIM-7.0
REFERENCE_FEATURE_GROUP_ID1 Associated ID of the classification system
z.B. 45-36-89-74 oder 21040701
TAX Tax
WA_NR Customs tariff number

SUPPLIER_AID is mandatory information, all further columns can be used as required.

A conditions file with price information is shown in the following example:

Beispiel eines Conditionsfiles

Structure of a conditionsfile (Excel view)

Explanation of the individual columns:

  • SUPPLIER_AID -> Supplier item number
  • LOWER_BOUND1 -> 1st price scale
  • NET_LIST1 -> Purchase price for the 1st price scale
  • LOWER_BOUND2 -> 2nd price scale
  • NET_LIST2 -> Purchase price for the 2nd price scale

Saving as a CSV file

After editing, save the Excel table for safety. Next, export the data as a CSV file:

File > Save as > File type: „CSV (separator-separated) (*.csv)“

Naming of the file:
catalogueID_conditionsfile.csv

Notes:

  • The catalogue-ID will be provided by Mercateo
  • Please keep the file naming. Without correct naming, the CSV file can either not be processed or not be assigned to the correct catalogue.

If you can export the CSV file directly from your system, you do not have to use Excel to create it.

Requirements and notes

Requirements:

  • Only semicolons are permitted as a separator.
  • The number of semicolons must be the same in every row.
  • The spelling of the headers cannot be changed.
  • Please note the use of capital letters within the headers.
  • A separate conditions file is required for each catalogue.

Information about price information

  • If you use bulk prices, the price must become smaller as the price scale increases.
  • Only the items for which a valid price is saved in the conditions file are put online.
  • The price must match the order unit in the catalogue.
  • For exclusive catalogues, please use net_customer as a price type (column header: NET_CUSTOMER).
  • For Mercateo catalogues, please use net_list as a price type (column header: NET_LIST).

This is what a correctly created conditions file could look like in a text editor:

Beispiel eines Conditionsfiles (Texteditor)

Example of a conditions file (text editor)

Activation in the Mercateo system

  1. You first create a conditionsfile according to the requirements above.
  2. Send this CSV file to support@unite.eu for check. Please indicate in the mail for which catalogue you would like to activate the file.
  3. Mercateo checks the file and makes all necessary settings in the system.
  4. You gain catalogue preview, can check everything and release the CSV file for the catalogue..
  5. Mercateo informs you about the next steps (naming regulation, transfer via FTP etc.).

Conditionsfile as whitelist

Besides updating product information and conditions, you can also control the visibility of the products on the Mercateo platform using a conditions file. A whitelist does not necessarily have to contain product information and can only consist of one column with the corresponding item numbers.
You can find more information about the whitelist here.

If you would like to activate a whitelist or set your conditions file as a whitelist, please write to support@unite.eu.