Each ARTICLE_PRICE element can specify a different price for the item. The following elements are secondary and are also supported in the Mercateo system:
→ PRICE_AMOUNT (mandatory field)
→ PRICE_CURRENCY (mandatory field)
→ TAX (mandatory field)
→ PRICE_FACTOR (not supported)
→ LOWER_BOUND
→ TERRITORY (not supported)
Extract from BMEcat:
<ARTICLE_PRICE price_type=“net_list„> <PRICE_AMOUNT>50.00</PRICE_AMOUNT> <PRICE_CURRENCY>EUR</PRICE_CURRENCY> <TAX>0.19</TAX> <LOWER_BOUND>1</LOWER_BOUND> </ARTICLE_PRICE> |
You can find further requirements with regard to price information in the table below.
BMEcat element | Requirement | ||||
price_type | → Mandatory field → If not otherwise agreed, the purchase price should be provided as:
→ If you additionally want to specify the Mercateo Auction price, please use:
→ For exclusive customer catalogues, please use:
→French suppliers can additionally specify eco_tax ➤ here, please use:
|
||||
PRICE_AMOUNT | → Mandatory field → The amount of the price is determined in the field PRICE_AMOUNT → A dot is used as a decimal separator → The price can be given with a maximum of 2 decimal places → The price is to be saved without VAT |
||||
PRICE_CURRENCY | → Mandatory field → There is a list of the currently valid currencies and abbreviations at https://en.wikipedia.org/wiki/ISO_4217 → The currency and VAT in the catalogue belong together. Please do not use currency and tax for different countries within a catalogue → The currency must correspond to the country the catalogue is activated in |
||||
TAX | → Mandatory field → TAX must occur exactly once in each ARTICLE_PRICE → The tax rate states the factor for VAT that applies to this price → Please show the tax values as decimal numbers. For 20% VAT, 0.20 should be stated in the catalogue → A dot is used as a decimal separator → The currency and VAT in the catalogue belong together. Please do not use currency and tax for different countries within a catalogue → The tax must correspond to the country the catalogue is activated in |
||||
PRICE_FACTOR | → This information is not supported at present | ||||
LOWER_BOUND | → Bulk prices ➤ can be shown using the element LOWER_BOUND → The lower boundary for the respective bulk price is defined in LOWER_BOUND → The first LOWER_BOUND should correspond to the minimum order value → Please only use positive integers |
||||
TERRITORY | → This information is not supported at present |